This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61201 75 uA quiescent current

Other Parts Discussed in Thread: TPS61201

Hi,

    I am designing a battery powered circuit in which the sleep mode current should be as low as possible.  I am using interrupt wakeup on a microcontroller. This device will take maximum current of around 700mA for short time when it wake up. But mostly it will be in sleep mode, so the controller takes at max 1uA. But  the 70 to 75uA quiescent current is a problem... What can I do in this situation? I followed the recommended layout for TPS61201 as far as possible but I am getting a quiescent current of 70 to 75uA. Since I am using lipo battery (100mAh) I need to regulate the o/p voltage to 3.3v because most of the components need 3.3v.