I need to drive a distributed ceramic capacitive load of ~80uF, 144 capacitors across a 1 sqft multi-layer PCB. Can I have a tantalum close to the LM2991 for stability, then add a series resistor before I drive the output power plane and the 80uF. The resistor's purpose is to isolate the low ESR ceramic capacitance to keep the LDO stable. I'll be using VIN = -15V, VOUT = -14.5V, I = 800mA. I can tolerate the IR drop of the resistor.
Quote LM2991 datasheet :
Ceramic Bypass Capacitors
Many designers place distributed ceramic capacitors whose value is in the range of 1000 pF to 0.1 μF at the
power input pins of the IC's across a circuit board. These can cause reduced phase margin or oscillations in LDO
regulators.
The advent of multi-layer boards with dedicated power and ground planes has removed the trace inductance that
(previously) provided the necessary "de-coupling" to shield the output of the LDO from the effects of bypass
capacitors.
These capacitors should be avoided if possible, and kept as far away from the LDO output as is practical.