Hi, I built three power supplies with the TPS54386. One is a 12V-5V and the other two are 5V-3.3V. One of these three does not seem to work. When I connect the input power, the chip gets really hot and there is nothing on the output. The other two (12V-5V and the other 5V-3.3V) are working fine. I checked all the component connections and their values too. I also checked for accidental shorts and other such incidents. Everything seems to be great with the board. Also the other two were tested with the same supply and under the same load conditions. What am I missing here?