This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2556: what is the purpose of two inputs

Other Parts Discussed in Thread: TPS2556

Hi folks,

I was checking TPS2556/7, this may be very naive question, but I am curous to know about the purpose of two inputs in tps2556/7. Does this package contains two independent blocks? Maximum total input voltage is 6.5 so if I am giving 3 to both input, would it add up to 6 or its a package of two ckts with two outputs? I checked datasheet, and is not explaining about this, I believe. And if i am giving only one input, Would it give same voltage at both the outputs?