Hi,
Assuming having the below inputs:
VBAT is set to 4.0V
IBAT = 325mA
Isys = 1.25A
So Isw = IBAT+Isys=1.575A
- What is the voltage Vsys – Is it VBAT + 3% -> ~4.1V
- What is min VIN which can be used in this condition?
- I do not see any efficiency parameter -> What is Iin at these condition?