Hello,
In a custom design we have detected a layout bug in realtion to the TPS84320.
The PH pins 10, 11, 12, 13, 14, and 17 are floating but not connected to the small copper area of the PH pin 46.
The datasheet mentions that all these pins are used for thermal relief.
Assuming that the maximum expected current consumption is about 1.5A, is there a relevant penalty with this connection??
Is it possible that with the mentioned conenction of these pins the regulator does not work properly??
Thanks in advance,
Antonio Mollfulleda.