I am using the bq24086 in a charger cradle. To protect the battery there is a series diode between the charger and the battery. If I take the feedback from the battery side of the diode back to the BAT pin, will the charger be stable? What value series resistor can I have between the BAT pin and the battery (is there a load current on the BAT pin or stability issues?)
Secondly, What is the bq24086 dropout voltage at lower currents? the datasheet only gives 600mV at 0.75A. Is the dropout much less at 100mA? A graph would be helpful.