The datasheet of the LMZ23605 stated on page 17:
"Additional bulk capacitance with higher ESR may be required to damp any resonant effects of the input
capacitance and parasitic inductance of the incoming supply lines. The LMZ23605 typical applications schematic
and evaluation board include a 150 μF 50V aluminum capacitor for this function. There are many situations
where this capacitor is not necessary."
Is this 150uF cap really necessary? Can you list some applications where this will be required? I may have a height restriction for the recommended Aluminum capacitor. If this required, is there an alternate capacitor type that will perform similar to the 150uF aluminum?
Thanks.