Hi,
In the user guide of LM3405XEVAL (snva222a), on first page, it states that this device can be configured to accept Vin from 3V to 5V. But it also states that Vboost - Vsw has to be in the range 2.5V - 5.5V in order to ensure gate drive voltage.
Questions:
- Does this means at Vin=3V, the Vf of LED can only be 0.5V ?
- Can I drive a 3V /1A LED with LM3405 at Vin=3.5V or 4V ?
- For Vboost - Vsw, what is the definition of Vsw, is when the switch is turned on ?
Regards,
CM.