Hello,
I wanted to ask if it is possible to implement a bidirectional controller with the UCC28950.
If not I would be very interested, if there is any other chip for this application?
Thanks in advance!
Best Regards
Uli Bürger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I wanted to ask if it is possible to implement a bidirectional controller with the UCC28950.
If not I would be very interested, if there is any other chip for this application?
Thanks in advance!
Best Regards
Uli Bürger
Perhaps I should dicribe a little bit more in detail what I want to do:
I have a high voltage battery and a high voltage DC-supply and I want to transfer energy between the battery and the DC supply (charge and discharge).
The battery-voltage is in full state round about 300 V and in empty state round about 200 V and the DC supply has a typical voltage of round about 330 to 350 V.
A typical application for bidirectional DC-DC-Converters with pretty similar in- and output datasets is the use in an electric car for driving the motor or to put the brakeenergy back into the battery.