Hi
Our customer need 180mA flash current (20mA Torch) setting, but this device set limiting minimum 200mA.
Can we lower current setting by external circuit?
Regards,
PAN-M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Our customer need 180mA flash current (20mA Torch) setting, but this device set limiting minimum 200mA.
Can we lower current setting by external circuit?
Regards,
PAN-M
Hello,
At first glance, this external circuit looks like it could work. This is something I have never tried. I would worry about temperate variations causing the LED current accuracy as well as the part to part accuracy to become reduced. As the temperature increases the LED VF will drop and make the current in the LEDs increase.
Plus, this external load is going to cause a pretty large hit to the solution efficiency (throwing away 10% of the current).
Can the customer use a parallel LED architecture? If so, a part like the LM3646 could be an option.
Greg Lubarsky
Thank you for answer.
Our customer cannot change to parallel LED because serial LED is module.
Do you have any other idea?
PAN-M