Hi,
I'm looking for an application note, describing the SEPIC configuration of the LMR61428. As mentioned in the datasheet the LMR61428 could be configured as a SEPIC converter. I will need to have it working for the following parameters:
Vin MIN = 3.3V
Vin MAX = 12 V
Vout = 5V
Iout 1.5 A
Thank you for your kind support