Have a customer trying to better understand the relationship of the Current Limit threshold versus opterating temperture of the IC. Here is the CL threshold data they have collected:
- 5A at 27C
- 3.3A at 70C
- 2.4A at 85C
They have conducted tests make help understand the behaviour of TPS40055 at temperature.
-
One characteristic was that the pulses broadened slightly near CL.
-
Another characteristic was the increase in phase lag between the beginning of the pulse and the Scope trigger.
-
One other characteristic was the increase in the negative excursion of the noise voltage of the LDrive (Pin 10) at the beginning of its pulse (i.e. turn-off of the HDrive) - but this was in the nano-seconds timeframe. Not sure if the device was actually current limiting, or else it was thermal limiting.
-
Monitored the IC surface temperature, but again there was no big revelations between low current and high current - about 8C degrees rise in both cases.