This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2543 DCP auto

Other Parts Discussed in Thread: TPS2543

Hi

I have aquestion about TPS2543.


Question

Handshake will be required even if if we will set DCP auto?
I think when DCP auto, D+ output 0.6V and short 200Ω return to D-.
So I think DCP auto dont need handshake.

So i think only if we change to CDP/SDP need the handshake. It is right?

Best regards,

masa

  • The handshake depends on the protable device.

    TPS2543 DCP_Auto integrate divider 1, divider 2 and shorted mode, for non-CF device, need handshake or enumeration signal to complete the mode change.

    For CDP/SDP, need handshake to distinguish CDP and SDP.