Hi guys,
Please advice could TPS63061 withstand continuously 12.6V supply voltage and 1A output current?
The application working range is 4.2V - 12.6V, which means a pure DC-DC Buck can't be used.
Although it is rated to 12V max, according to the Absolute maximum ratings Vamax is 17V.
Here we're talking about 0.6V above the 12V limit ( 3 x Li-Po ).
The problem is that the design has been finished and the working range of 4.2 - 12V has been tested, but with fully charged Li-Pos, the max voltage will become 12.6V.
Best regards
Nick