Hi guys,
I am working on a project, using the LM3409 buck converter.
The constraints are:
Vin 12 - 40V, Vout: 9V, Iout: 1-5A, frequency: approx. 500kHz.
Shunt: 47m Ohms
Coff: 2nF, Roff: 220 - 10k Ohms.
I simulated the project, and everything was fine.
When I built it, I saw that there are several very short on- and off- switching states within one free-wheeling cycle. The time between them is approximately the off-time.
Now I red the datasheet, and that says, that the LM3405 switches the + and - comparator inputs with every cycle - leading to an offset of 24mV.
-> the current has to decrease by more than 0.5A before the next switching cycle - if a shunt of 47m Ohms is used.
The problem is still there, if I make sure, that the current deccreases more than 0.5A before the off-time ends.
This is a problem, because it leads to a very high inductor current ripple and to many switching cycles, which leads to a thermal problem of the switch.
If the current is reduced, or the off-time is reduced, the switching cycles within one free-wheeling period become less.
You can see the volatage and the current in the inductor in the picture attatched.
Does someone have an idea where this problem might come from and what could be done about it?
Did anyone have a similar problem?
Thanks,
Philipp