how do i get 22 vdc out of this device. i followed the wiring per data sheet. i only get the source voltage on the output.
15v input 92 ohm pin 7 to 4 i'm getting 15 volts out.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In order to set the output voltage to 22V, the minimum input voltage must be Vin=(Vout+4).For 22Vout, minimum vin is 26V and maximum vin=36V.
Note 2 in the PTN78060H data sheet, For output voltages of 19 V and higher, the minimum input voltage is (VO + 4) V. See the Application Information for further guidance.
Maximum ouptu current at 22V is 2Amps
Tom
The PTN78060W is a buck step down regulator.
The PTN78060A is a buck boost , + Vin to (-) vout maximum ouput voltage is (-15V).
Note 2 PTN78060A specification
(2) The maximum input voltage is limited and defined to be (32 - |VO|).
Tom
so. is the ptn78060a what i want to use to rise the power supply voltage from 12vdc to 24ish vdc. ?? i like the power supply that i'm using, but it's 13 vdc. the amp requires 24 vdc. ..
PTN78060A absolute maximum (-) output voltage is limited to (-15V). With (- 15V) Vout, input voltage range is minimum +9V to maximum +17V.
Tom