Good day to all ,
Please i need your help on how to calculate the correct value of External Pull-Up resistor to be used for the Output channels in TLC 5971 chip.I have 4 pieces of tlc5971 on my board.the voltage supply to each chip is 4.1V(Vcc-Pin19)while my IREF(Pin1) is 24.8k Ohms.
I am using the signals generated from the tlc 5971 to modulate the pwm of an Led Driver with a constant current Output of 700mA and 3.8V which is used to control the brightness of Hihg Power Leds.The Problem i am having is that the PWM Signal is not stable and clean.
For instance when i used 3.9k Ohms for the Pull Resistor,the Leds were ON only @ 5% and there was error of 3% but when i used 1.5K Ohms for one of the channels,the Led was ON @ 1% and at the same time the error was reduced to 0.07%.Because of this result.i changed all the Pull-Up resistors to 1.5k Ohms but to my suprise all the Leds did not ON,so i have to Change the Pull-Up resistors back to 3.9K Ohms.
Sir,I would be very glad if you could guide me on how to calculate the correct value of the Pull-Up resistor taking into consideration the Information i provided above.
thank you for the usual Support. Best regards