This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HUM noise in BQ24167 & TPS2500 based charger ckt

Other Parts Discussed in Thread: BQ24167, TPS2500

Hi,

I am using BQ24167 dual input charger IC & TPS2500 USB Boost converter in my charger design.

I am able to hear HUM sound from the system.(Mostly near Input section of TPS2500 )

Block Diagram:- 

Circuit :-

While probing battery voltage (when Hum sound is resent) i am able to see max 560mV fluctuation on bat+.

Plot:-

Battery Signal levels for Samsung Galexy mobile load are,

Battery Spec:- 3.7V / 3Ahr Li-ion battery.

Bat Voltage = 3.59V 

Load current =510mA (To mobile)

Noise Amplitude=440mV

Noise Frequency= 4.0KHz (Frequency of the signal will vary depends on Load current & battery % based on this I am able to here different hum sound ).

 

TO Reduce Noise :-

I tried to change TPS2500 inductor from 3.3uH to 2.2uH. --> Still noise is present.

I added 150uF bypass cap on Battery node.--> Noise ampletude reduced to half.(but still low sound noise the present)

Pls help to solve this issue.

Thanks in advance.

 

Regards

Raj