Other Parts Discussed in Thread: BQ51013B, BQ51013BEVM-764, BQ500211, BQ51003
Dear sir or madam,
I want to develop a system to transfer wireless power. I want to use the wp-receiver as a constant power supply for a sensor. I won't charge a battery or anything like that. The receiver should be a voltage source. It is not important to me, that the application is Qi compliant. I'dont care about that. I've found the following reference design: http://www.ti.com/lit/an/slua705/slua705.pdf
This is more or less exactly what I'm looking for. But I've several Questions.
1.) Question: Is it possible to use ti controllers lik a bq51013B for power supply only? I guess yes.
2.) So I'dont really need the communication. Is it possible to shut down the communication and use the controllers without?
3.) The reference desgin "low power transmitter" (see the link above) uses another coil than usual but with the same value: 6,3 µH. Why is the transmitted power less than 2.5 W? I don't understand it: Nothing changed?!?
4.) Again to the reference design: Can I use a standard receiver like a bq51013bevm-764 together with the low power solution with the bq500211? Will it work just with a lower output current? Or do I have to develop a special receiver?
5.) Würth Elektronik will release some new coils soon. Receiver coil size: 10mm. I'll use them for my application. So can I just use a bq51013b, change the receiving coil, change the resonance capacitors --> so that all together has again a resonant frequency of 100kHz and it will work?
6.) For me it is difficult to understand, when will the communication protocol fail. So what are the minimum/maximum ratings for AC1/AC2 at the receiver side and the minimum/maximum ratings at the transmitter side of the coil that your firmware will still work. How can I figure out that?
7.) Can I use every coil I want as long as I have the correct resonant frequency and a voltage of at least 5V?
You would help me a lot with your answers.
Sincerely yours
Sebastian Heinrich