Hello Friends,
Pls help interpret the attached waveform. Why is the waveform getting chopped from top... how to resolve it.
Maverick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
It is very quite out here. Let me elaborate on the problem that I am facing.
I have designed a led driver using TPS92210 to output 75V / 600mA. Input range I intend to operate is 100VAC to 300VAC.
The transformer has turns as mentioned below...
Pri: 28 Turns; Sec: 28 Turns; Bias 12 Turns; Core: PQ2620; Freq 85 KHz; On_Time: 4.5uS.
Leaving alone the spike or overshoot, I am expecting max Vds @ 295V to be around 495V and measured also is close to that. The relaxation ring caused by the parasitic / stray capacitance is getting chopped off. I have captured (@295VAC) the Vds waveform and attached for your reference.
What want to know the reason why it is getting chopped off and would it make my board unreliable.
Pls reply
Maverick