This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED driver

Other Parts Discussed in Thread: TLC59116F, TLC59116FEVM-571, TLC5949

Hi,

I am working on a project that needs an LED driver.  If you can help or point me in the right direction I would appreciate the help.

I like the constant current sinks in the TLC594x and TLC59116F family of parts but I am going to have some questions and will get an EVM to borrow and play around with.

I see that TLC59116FEVM-571 is available are any of the TLC594x EVM boards going to become available too.

Here are some specs on what I need.

  • 12-14 channels (strings)
  • 30mA per string
  • 10.2V peak voltage per string, 9.15V typical.
  • Need brightness control such as PWM.
  • Low Control Voltage
  • Small package QFN24 would be nice.
  • Battery operated  ( 4400mAh 7.4V Battery )

I would like to keep the voltage headroom as low as possible to keep the power down.  This means the current sink pins need to have a low regulation voltage.  A lot of these parts aren’t exactly clear on this point as to what the voltage is although many of them seem to want about 1V.  With 14 channels 100% duty cycle at 30mA and 1V control voltage on each current sink pin that is 0.42 W.   Would like to get that down.

  • Hi Calum,

    Most of TI's LED driver is 16CH, of course, also have 24CH and 48CH. Most of them can support 30mA. If you need PWM control, just choose a PWM part, such as TLC594X. This family are all 16CH PWM LED driver.

    For the requirement of LOW control voltage, you can get the information from V-I curve in datasheet. In fact, the minimum control voltage will change with the sink current.For our lastest part, it can support 0.22V @10mA.

    Hope it is useful for you.

     

  • Thanks,

    If I look at the TLC5949 as an example - I'm looking at Fig 13 output current v output volatge. The test conditions for this graph are.

    Vcc = 3.3 V

    BC = 7Fh

    Voutn = 0.8 V

    TA = +25 C

     If VoutN is set at 0.8V as the test condition(I assume that's the volatge on the 16 OUT pins)-  what is the output volatge along the x axis in te graph telling me?

    Cheers

    Calum

  • Hi Calum,

    It is a little confusing. Voutn = 0.8V means other channels except the measured channel is set to 0.8V. The measured channel change from 0V to 3V. So you can get pin voltage in this graph.

    Cheers,

    Rosley