Dear All,
Would you provide us the specification data of TPS62560?
Please give us the data which can show accuracy of TPS62560's Vout, at following situation.
Vin :3.3V
Vout :1.2V
Iout :300mA
It is written as "Output Voltage Accuracy in PWM Mode ±2.5%" to a datasheet of TPS62560.
However, our customer is interested in a competing IC of "Output Voltage Accuracy ±2.0%".
Will you provide to us measurement data of this IC's several lots?
Best Regards,
Tsuguhiko Asai