Hello,
I am working on a design that will use the TL5001. It is a DC-DC high Vout flyback converter. Unfortunately, the datasheet does not specify if a flyback configuration is inherently possible with this chip hence my enquiry if a similar design exist.
On a side note, even a simple test start (using dummy 1V on FB pin) is proving difficult at this stage. It seems to me that there is an internal condition not set correctly which prevents the output from switching.
Any help would be appreciated.