Other Parts Discussed in Thread: TWL6040, TWL6041
Hi All,
We are using AUXLP/AUXLN lineouts of TWL6040 to drive a Class D amplifier in our design.
In order to set the gain in this path to achieve 3.5W we have he following Queries:
(1)The power supply to PGA is 1.8V(from HSLDO)and -1.6V(from LSLDO).The maximum output swing from PGA can be within (1.8-(-1.6))=3.4V
Converting this to Vrms translates to ((3.4/2)/sqrt(2)) which will be 1.2V Vrms.
However, in "AUX-Output Path Specification" (Pg 23) for TWL6041(literature no: SWCS066C REVISED JANUARY 2012),
Output differential swing @ 0 dBFs,THD < -40 dB,RL = Typ is 1.7 Vrms(minimum).
How can we get this minimum of 1.7V Vrms with +1.8 and -1.6V supply?
(2)In the figure "Figure 4-11. Auxiliary Outputs" the gain at the output of PGA is shown to be 4.6dBVrms.Is this the maximum gain that can be achieved?
If yes, the output Vrms swing on AUX lineouts for this gain will be 1.7Vrms(4.8V peak to peak).How is this achieved with (1.8-(-1.6))=3.4V supply?
(3)In the register "HFLGAIN" we can program the gain in steps of 2dB (-52dB:6dB). Can you please corelate this with 4.6dBVrms gain in the Aux path.
Also,What is the maximum Vrms output available on AUXL lineouts(considering 6dB gain)?
Thanks and Regards,
Naveen