Hi,
I am trying to drive constant 1A current using LM3405 connected to a single OSRAM IR LED "SFH 4715".
Below is the circuit using which I am trying to achieve the above:
Setup I used:
- VIN = 5V
- EN/DIM = TIED to 5V VIN DIRECTLY
- R1 = 0.2 ohms (Tolerance unknown)
- L1 = 10uH, 5.8A (Manf. part no: B82477P4103M)
- D1 = Manf. part no "PMEG3015EH,115"
- D2 = 1N4148
- C1 = 10uF/6.3V (X5R or X7R not sure, bought from local market)
- C2 = 1uF, 10V (X5R or X7R not sure, bought from local market)
- C3 = 0.01uF/16V (X5R or X7R not sure, bought from local market)
- C4 = 1uF, 10V (X5R or X7R not sure, bought from local market)
My Observations:
@ SW pin = getting ~90% duty cycle of 1.6MHz PWM output.
@ VOUT = 2.5V
@ VFB = ~0.2V
But the Current consumption of this setup is only ~200mA.
The OSRAM IR LED part I am using has forward current = 1A and forward voltage max 2.8V.
For you reference I am attaching the IR LEDs datasheet.
7180.OSRAM IR LED DATASHEET.pdf
I would like to know what could be limiting the output current to 200mA instead of giving out 1A.
Datasheet says, Iout = Vfb/R1 = ~0.2V/0.2ohms = ~1A.
L1 Inductor am using has good current capacity (5A). So this should not be a problem ?
I tried debugging this in following methods:
1. Check how much current the OSRAM LED takes, IF CONNECTED DIRECTLY TO POWER SUPPLY :
Varied the forward voltage from 2V to 4V. When >3V the LED started drawing huge current.
Does this mean, its forward voltage(max 2.8V) as claimed in its datasheet is wrong ?
Or did the LED got damaged and thus it was drawing huge current ?
2. Tried connecting another IR LED (OSRAM) in parallel to this. Still NO CHANGE. Vout = 2.5V and Iout = ~200mA.
It would be very helpful if someone could clarify.
Thanks and regards,
Karthik
+91-9944980621