Hi,
I would like to connect one or two DC PSUs to a buck switch in order to get both voltage level conversion and current sharing into 12V, 2*15A.
Am I right to suppose that a dual current-mode controller (e.g. LM5642, LM5642X, or LM2642) could be used? (Or two separate ones?)
This differs from the standard one-output design of LMx642 in the sense that the two V_in are separate.
The two DC sources are identical.
It would be a plus if it were possible to have only one DC source connected. (If possible - which controller channel would have to be used?)
Grateful for your input.
Thanks in advance.
Best regards
Niclas