This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I don't think that group monitors the forum very closely. Let me see if I can direct someone to reply.
Hi Yusuke,
I found following description in the datasheet:
"When the device is enabled there is an approximate time interval of 50 μs when the soft-start capacitor will be discharged just prior to the soft-start ramp. If the enable pin is rapidly pulsed or the soft-start capacitor is large there may not be enough time for CSS to completely discharge resulting in start up times less than predicted. To aid in discharging of soft-start capacitor during long disable periods an external 1MΩ resistor from SS/TRK to ground can be used without greatly affecting the start up time."
Which indicates discharge time should be around 50us, and you can add external 1Mohm resistor to speed up the discharge.
I am also trying to contact the orignal designer/apps engineer to see if they have more details.
Thanks.