This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54395- Designing Industrial power supply.

Other Parts Discussed in Thread: TPS54395

Hi

I am designing a two channel power supply, for that I have shortlisted "TPS54395"

Parameters of my power supply are:

Input = 12VDC, 2.5A/3A (SMPS)

Output= 3.3V, 2A and 4.173V, 3A

I have two questions regarding my designe. 

1) Does TPS54395 will restart if self from UVP, overcurrent and thermal shutdowns? Or will I have to restart it manually? 

2) Is my above calculation valid? That is is 12V 2.5A enought to get the output I want? 

3) I am planning to put 1000uF caps parallel at both outputs to avoid brownout conditions in microcontroller. Will this cap affect working of regulator?

Thanks