Please also include the following information:
Battery Chemistry: 1 sealed LEAD ACID BATTERY
Battery Capacity: 6 V, 7AH (PS-670, power sonic)
Desired Charging Rate: Charging 8 hour and discharging 6.5 hour
Charging current max <2A from source.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI,
I have 12V input DC source and need to charge 6Volt battery. We had used UC3909 (out pin) switch mode option(Buck) and drop the voltage as per requirement.
Is that Bq2031 can do this job? Please give me some reference.
If not please suggest another IC to do as per my requirement.
Please also include the following information:
Battery Chemistry: 1 sealed LEAD ACID BATTERY
Battery Capacity: 6 V, 7AH (PS-670, power sonic)
Desired Charging Rate: Charging 8 hour and discharging 6.5 hour
Charging current max <2A from source.
How UC2909-EP(Active) IC is compatible with UC3909DW(lifebuy). Please suggest.?
Thanks,
Ashok