Hello,
Vcc and DR pin absolute maximum ratings are 6V.
However, Vcc and DR pins will be 6.2~6.3V at the condition of the following.
However, Vcc and DR pins will be 6.2~6.3V at the condition of the following.
This voltage is larger than absolute maximum ratings.
Are there any problem in this condition?
Are there any problem in this condition?
If yes, could you please let me know the workaround?
<Conditions>----------
LM3481SEPICEVAL/NOPB
LM3481SEPICEVAL/NOPB
Vin=6.1V
Vout=5V
Iout=250mA
-----------------------------
Please see the attached file as Vcc pin and DR pins waveform.
Since these pins are output pins and VDR(max) is 6V(typ), I think that we can accept these voltage.
We should care the absolute maximum voltage for input case.
We should care the absolute maximum voltage for input case.
Best Regards,
Ryuji Asaka