Hi all,
I try to implement this source for our sensor. we need to have 0,5-8mA at the Sensor. I don´t know if it is really good to use this component, maybe it is better to use the LM317. Or something completly different?
greetings Rainer
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I try to implement this source for our sensor. we need to have 0,5-8mA at the Sensor. I don´t know if it is really good to use this component, maybe it is better to use the LM317. Or something completly different?
greetings Rainer
Rainer,
What is the desired output voltage?
What is the minimum and maximum input voltage?
Hi Ronald,
i have solved the problem already, it was the wrong ic... i work at the moment with LM317, but the LM is very noisy, do you have for this a solution?
Rainer,
It is incorrect to short ADJ and OUT pins of the LM317.
A linear regulator can't output 24V with a 16V to 32V input.
For a linear regulator VOUT will be less than VIN.