Hello,
I am new to the Audio Systems design, I am designing the OMAP4460 based SBC. From datasheet it's known that the TWL6040 IC can drive Stereo Speakers 8 Ω, 1.5 W per Channel. I need to include the on-board speaker and microphones (instead of jack connected external speakers/microphone).
Which speakers would suffice (with 5meters range @ 70-80db max)? (Any reference design or part number would do.)
Thanks in Advance.