I'm calculating the minimum output capacitance of a a design using the datasheet guidelines, document SNVSA09B, Section 9.2.2.5 'Output Capacitor Selection'.
The resulting values I'm getting are in mF and even if I input the design example values (into Eq 19) I can't get even close to the 141uF result of the design example. I had another engineer here check to make sure I wasn't doing something really stupid but we both ended up with similar results.
Vin = 12V
Vout = 4V
Iload = 2.4A max
Resulting values:
L = 4.7uH
D = 0.33
Iripple = 430mA
Co = ??
Does anybody have any idea where I'm going wrong with these equations? There are a little different to what I'm typically used to seeing on TI datasheets for output capacitance. I've noticed a slight circular dependance in that the output voltage ripple is used to calculate the capacitor value (Eq 19) and the capacitor value is used to estimate the output voltage ripple (Eq 17 and Eq 18).