I just picked up one of these PoE PD eval boards, and have a question. I don't see any information on the data sheet (for the eval board or PoE controller / DC-DC converter) for adjusting the output voltage. I assume since max duty cycle of the DC-DC converter is nearly 80% a wide range of voltages should be realizable. Usually there is an equation for calculating feedback resistances to set desired output voltage. Am I missing something obvious? While I actually want the 12V output the board is designed for, I'd like to know about this. I have read the threads on both the 23754 and 23756 here without finding what I'm looking for.
Thanks for your help.