I'm trying to use an LM22671 (the fixed 5.0v version) in an automotive (+24v) application to generate a voltage rail at something like +7V. From looking at application notes, it would appear that the minimum voltage to keep the output in regulation is at least 1.5v higher than this. What happens when the input is less than this value (and thus the likely off time of the switch is less than the datasheet requirement)? I have a prototype circuit which is largely working; if the supply is reduced from 12v down, the output remains at the regulated voltage until the point at which it cannot regulate, then the output follows the input downwards within 0.2v (presumably with the switch turned on 100%). If the input is reduced below the UVLO threshold, the device shuts down the output; if the input is slowly increased from zero, it does not then start up. How can I guarantee startup (eg by increasing the UVLO threshold by external resistors)?