- I have prototyped a solution using the LM3478EVAL board.
- The device produces audible noise in the 5-20kHz range due to OVP under light loads.
- I am skeptical that reducing L and utilizing DCM can reduce the output current to below my minimum current requirements which are likely to be in the 100mA range due to the minimum D=0.325 (325ns blanking / 1000ns PWM period.)and provide adequate throughput to produce the 5-10A of output current required at high loads.
- Is there another solution in the TI controller family that can accommodate this range of output current requirements without producing audible noise?
Thank you in advance for your help.
Bryan