Hi,
We're experiencing some issues with the LM25011Q1MY/NOPB part, a switching regulator. The most typical failure mode is that there is no regulation, i.e. that both the output voltage and current are not regulated. There is some dropout, but otherwise the output voltage essentially tracks the input voltage. This device is being used to charge a 4-cell Lithium battery, so we are concerned about excessive current, and especially over-voltage conditions. Another failure that was seen recently is the chip presents a short to the input supply voltage.
After some troubleshooting, we determined that, after the part stops regulating, the Feedback Voltage (out of pin 6) is ~3.35V (instead of 2.51V) and the chip is not switching on pin 9 (constant on). This was with an input voltage of 24V and designed to regulate 16.6V out.
I've attached the schematic of the control circuit we're using with the chip. Any insight into why the chip would keep failing like this?
Thanks