I would like to ask about PMP7499 circuit design.
In the PMP7499 schematic (slvrb55), there is no termination circuit at the PoE+ magnetics center tap of data port side. Is there any reason why there is no? Isn't it needed? or should the customer set the termination circuit?
And also, about ETHERNET POWER port side center tap termination circuit, how can we decide these R, C component value and voltage and power rating? (It is 0.01uF/100V, 1000pF/2kV and 75ohm/ 1/16W)
Best Regards,
Kohei Sasaki