Dear all,
Please teacn me about BQ500212A.
http://www.tij.co.jp/general/jp/docs/lit/getliterature.tsp?baseLiteratureNumber=sluuap8&fileType=pdf
Q1, What is the function of SNOOZE_CHG and SNOOZE_CAP?
There is the circuit connected with SNOOZE_CHG and SNOOZE_CAP.
What is the mean of this circuit?
Q2, BQ500212A's datasheet say 'SLEEP pin connected to 5s interval circuit' and 'SNOOZE pin connected 500ms interval circuit'.
Where is the part that substantiate this connectivity in EVM board?
I guess R53/C32 and R25/C22 each substantiate interval circuit. What is the way to calculate these values?
Q3, Can we use transistor in place of CSD97376Q4M?
If this is possible, should we set 'Base:PWM signal / Collector:VIN / Emitter:Tx Coil' ??
Q4, How can we use JTAG and DATA signal?
Datasheet say these pin are used for debug. But, what can we do in the concrete?
Best regards,