Having trouble with a string of bq76PL536a devices in which only the first device in the chain will exit sleep mode. Is there a trick to this? Are you allowed to use the Broadcast address to enter/exit sleep?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Having trouble with a string of bq76PL536a devices in which only the first device in the chain will exit sleep mode. Is there a trick to this? Are you allowed to use the Broadcast address to enter/exit sleep?
To exit from sleep mode, the following sequence should be executed:
Thanks, Stephen, but that does not seem to be working for me. The host SPI CS is asserted by the SPI interface routine. As an interesting(!) side effect, once commanded into sleep, because of my error a device won't even respond to BQ76PL536_RESET, so there's the possibility of bricking battery packs. Here's my code:
bool bq_pack_Sleep_Exit(void) {
uint8_t Device;
bool Success = false;
for (Device = 1; Device < NUMBER_OF_BQ_DEVICES + 1; Device++) {
spi_write_reg(Device, IO_CONTROL_REG, 0b00000011); // TS1&2 power on, Sleep off
// According to Battery Management - Gas Gauge Forum note, need to wait at least 1ms between subsequent wakes
while (false == SecondsFlag); // wait here 250ms, 63ms not enough? Try one second
SecondsFlag = false;
spi_read_reg(Device, IO_CONTROL_REG, 1, DISCARD_CRC, &SPI_Data[0]); // Read-back IO Control
printf("Sleep exit, Device %d IO Control read-back 0x%.2X ", Device, SPI_Data[FIRST_VALID_BYTE_INDEX]);
spi_read_reg(Device, ADC_CONTROL_REG, 1, DISCARD_CRC, &SPI_Data[0]); // Read back ADC Control
printf("ADC Control 0x%.2X ", SPI_Data[FIRST_VALID_BYTE_INDEX]);
spi_read_reg(Device, ALERT_STATUS_REG, 1, DISCARD_CRC, &SPI_Data[0]); // Check Alert Status
printf("Alert Status 0x%.2X ", SPI_Data[FIRST_VALID_BYTE_INDEX]);
// Acquire alert and fault status and clear if any have occurred
Clear_Fault[Device] = clear_faults(Device + 1, &Device_Status[Device], &Fault_Status[Device],
&CUV_Fault[Device], &COV_Fault[Device], &Alert_Status[Device]);
printf("Status: 0x%.2X Fault: 0x%.2X Alert: 0x%.2X\r\n",
Device_Status[Device], Fault_Status[Device], Alert_Status[Device]);
}
return Success;
}
The above queries to the Sleeping device return zeros. I can see that the device is actually in sleep by the bench supply current.
Can you see what I'm doing wrong? Thanks!
One other intriguing thing -- when Device 2 is commanded into Sleep mode, and before the next lower device is commanded, the IO Control register can no longer be read back after about 50ms (more than 25ms but less than 1 second). This in spite of the datasheet note that says in Sleep mode, " SPI communications are preserved; all registers may be read or written." Device 1 in Sleep mode does allow continued queries of the IO Control register.
I'm not sure what you are doing wrong, but I can read the IO_CONTROL register in each device in a 3 IC stack 100ms after they have been put to sleep. I can verify the ICs are still in sleep mode by the current consumption.
Is there a way we can dialog more directly, so I can send you schematics and so on?
I've refined my tests and found I can no longer read IO_Control on Device 2 after 500ms +/-50. But it seems key to me that communication is lost on Device 2 after that point, so that it cannot respond to clearing the Sleep bit.
So are you saying that even with the entire 3-device stack in sleep mode, your test on the Evaluation Module shows you can always access all devices in the stack? Able to read Device 3 when lower two devices are in sleep mode? My problem is that I can't read Device 2 in Sleep even with Device 1 awake.
My BMS is arranged with two devices per board, and intended to chain additional BMS units above. I believe I've matched the Evaluation Module schematic for the interconnection and termination.
You can add me as a friend, then we can privately message each other.
Yes, I can confirm that I have a 3 device stack (the EVM board) with each device placed in SLEEP mode, each with a different configuration in the IO_CONTROL register: ID 1 has 0x04 (SLEEP mode only), ID 2 has 0x05 (SLEEP mode with TS0 enabled) and ID 3 has 0x06 (SLEEP mode with TS1 enabled). Without removing any devices from SLEEP mode, I then read back the IO_CONTROL register of ID 1, wait 100ms, read IO_CONTROL of ID 2, wait 100ms then read IO_CONTROL of ID 3. I get the expected values of 0x04, 0x05 and 0x06 (respectively).
Can you confirm that device 2 is responding before it goes into SLEEP mode?
To close this query out, the problem was caused by using the Reg50 signal to pull up the Hsel signal. Since Reg50 is disabled during Sleep, and Hsel when low switches to the Host interface mode, setting Sleep disconnected the Slave interface and cut off further communication. At that point, power must be removed from the chip to reset communications.
Regarding setting / clearing the Sleep mode discussed at the top of the thread, once the hardware error was corrected communication up the chain of devices is always enabled even in Sleep mode so a broadcast message clearing the Sleep bit in the IO Control register is effective, and the wait loop implied early in the thread does not appear necessary. Also, a broadcast sleep message can be followed by commands clearing the Alert bit set by entering Sleep mode for each device.