Hello,
I would like to know how does the BQ2050h determine the actual C-rating of a discharge.
I have a 4000mAh lead acid battery that has aged and is now yielding around 1000mAh of capacity. Observing the contents of FLGS2 register, it gives a DRATE result of less than 0.5C even when i discharge with a current of 2.4A.
I am not sure if the C-rating is determined from the current sensed at the SR input or from the LMD value.
Look forward to your replies