This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54494 stability

Other Parts Discussed in Thread: TPS54494

Hello,

I am trying to use the TPS54494 IC as a dual 3.3V / 5V power supply - with little success. The output is mostly stable, but every 20-30ms the IC seems to "stop switching". I have attached an oscilliscope reading:

There was very little load on the power supply (around 5-10 mA) when these measurements were made, additional load will increase the voltage drop during these phases.

I am using a 4.7uH inductor (Eaton DRA124-4R7-R) and a 47uF capacitor (TDK C2012X5R1A476M125AC) on both sides.

Any idea what may cause this problem? 

Thanks,
Bálint