This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2750 short circuit protection and output current control

Other Parts Discussed in Thread: LM2750

Hi,

I've noticed on the forums and datasheets that the LM2750 DC step-up regulator has output short-circuit protection.  Does this mean it also has input short-circuit protection as well?  

Also, is there a way to set the input and output capacitors so that I_OUT ~= I_IN, with the voltage still doubled and V_IN = 3V?  Phase delay is not an issue.

Thanks.