Hi all,
I'm powering the TLC5941 with 5V. So low level is 0.2Vcc (from 0 to 1)V and 0.8Vcc (from 4 to 5)V.
I want to interface it with STM32F4 ARM. It has 3.3V CMOS levels for output. The output high for it is Vdd - 0.4 = 3.3-0.4 = 2.9V.
Not enough for TLC. Is it possible to convert levels? Or the only way is to power TLC from 3.3V.
I saw i EVK board for TCL5941. It is powered from 5V and the CPU is on another board (TUSB3210). It is powered from 3.3V.
How the interfaces are combined there?
Thanks in advance