Our LM3431 application specification Vin 9V~16V, Vout around=42v 140mA/ch*3=420mA
when vin 9v, in=1.9A , currenst sensing resistor=25mohm , then we can hear the noise from the chock. but after increasing vin above 10V, then no noise sound heared.
Moreover, once we increase current sensing resistor =52mohm , same supply voltage(vin 9v) then, no noise sound heared.
why the sensing resistor will effect the chock noise?
Is there other way to improve this situation?
Thanks.