I use the TP65252 for power supply, like this
BLUK1 : 5V , 3A
BLUK2: 3.3V ,2A
but when the 3.3V load is up to 400mA ,the 3.3v is drop down with 10ms.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.