This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62110 / Use with LM10010

Other Parts Discussed in Thread: TPS62110, LM10010

Hi All,

Our customer has evaluated TPS62110 with LM10010 to adjust output voltage to control rotating speed of fan. Then how should we set the external component value especially inductor to get stable operation. Should it be set at highest Vout or lowest Vout? Following is their requirement.

Vin > 13V

Vout = 3V to 12V

Iout = 0.3A

Best Regards,

Sonoki / Japan Disty