Hello,
I use bq24192I. And I have two questions about the behavior of Safety Timer.
1. Are "start condition of Safety Timer" and "the state of the stop" correct, in follows?
(Conditions: VBUS=9V, VBAT=3.7V, the register setting of bq24192I is default)
- When /CE becomes Low(charge enable), the counter of the Timer starts.
- When the Timer is expired, EN_HIZ(REG00[7]) is set to "1" and the buck converter stops.
2. About restart processing after Safety Timer stop
- When /CE is changed from High(charge disable) to Low(charge enable), is the Timer cleared ?
Does the charging restart?
- If REG00[7] is set to "0", does the charging restart?
Regards,
Daisuke