This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boost cap between VBST and SW voltage rating

Other Parts Discussed in Thread: TPS62200, TPS562200

What voltage could be seen across the boost cap?

Assuming Vin is 12V, the wavefrom on the SW pin is 0 to 12V switching waveform. The VBST pin presumably has a voltage already on it, so that during the high cycle of SW, the VBST voltage can be pushed up for a source to bias the N-ch FETs. But how much?

If we're to allow for DC derating of ceramic caps, then the maximum voltage imposed across the cap is needed, so a cap of a suitable voltage rating and derating spec can be used.

The minimum required capacitance of the cap would also be useful. I didn't spot either of these in the datasheet (TPS62200).

Regards,
Lyndon